Load Cell
Introduction to Load Cells
A load cell is a transducer which converts force into a measurable electrical output. Although there are many varieties
of load cells, strain gage based load cells are the most commonly used type.
Except for certain laboratories where precision mechanical balances are still used, strain gage load cells dominate the weighing industry.
Pneumatic load cells are sometimes used where intrinsic safety and hygiene are desired, and hydraulic load cells are considered in remote
locations, as they do not require a power supply. Strain gage load cells offer accuracies from within 0.03% to 0.25% full scale and are
suitable for almost all industrial applications.
Wheatstone Circuit with Compensation
Learn more about load cells
Load Cell History
Before strain gage-based load cells became the method of choice for industrial weighing applications, mechanical lever scales were widely used.
Mechanical scales can weigh everything from pills to railroad cars and can do so accurately and reliably if they are properly calibrated and
maintained. The method of operation can involve either the use of a weight balancing mechanism or the detection of the force developed by mechanical
levers. The earliest, pre-strain gage force sensors included hydraulic and pneumatic designs. In 1843, English physicist Sir Charles Wheatstone
devised a bridge circuit that could measure electrical resistances. The Wheatstone bridge circuit is ideal for measuring the resistance changes
that occur in strain gages. Although the first bonded resistance wire strain gage was developed in the 1940s, it was not until modern electronics
caught up that the new technology became technically and economically feasible. Since that time, however, strain gages have proliferated both as
mechanical scale components and in stand-alone load cells.
Load Cell Operating Principles
Load cell designs can be distinguished according to the type of output signal generated (pneumatic, hydraulic, electric) or
according to the way they detect weight (bending, shear, compression, tension, etc.)
Hydraulic load cells are force -balance devices, measuring weight as a change in pressure of the internal filling fluid. In a rolling
diaphragm type hydraulic load cell, a load or force acting on a loading head is transferred to a piston that in turn compresses a filling
fluid confined within an elastomeric diaphragm chamber. As force increases, the pressure of the hydraulic fluid rises. This pressure can be
locally indicated or transmitted for remote indication or control. Output is linear and relatively unaffected by the amount of the filling
fluid or by its temperature. If the load cells have been properly installed and calibrated, accuracy can be within 0.25% full scale or better,
acceptable for most process weighing applications. Because this sensor has no electric components, it is ideal for use in hazardous areas.
Typical hydraulic load cell applications include tank, bin, and hopper weighing. For maximum accuracy, the weight of the tank should be
obtained by locating one load cell at each point of support and summing their outputs.
Pneumatic load cells also operate on the force-balance principle. These devices use multiple dampener chambers to provide higher accuracy
than can a hydraulic device. In some designs, the first dampener chamber is used as a tare weight chamber. Pneumatic load cells are often
used to measure relatively small weights in industries where cleanliness and safety are of prime concern. The advantages of this type of load
cell include their being inherently explosion proof and insensitive to temperature variations. Additionally, they contain no fluids that might
contaminate the process if the diaphragm ruptures. Disadvantages include relatively slow speed of response and the need for clean, dry,
regulated air or nitrogen.
Strain-gage load cells convert the load acting on them into electrical signals. The gauges themselves are bonded onto a beam or structural
member that deforms when weight is applied. In most cases, four strain gages are used to obtain maximum sensitivity and temperature compensation.
Two of the gauges are usually in tension, and two in compression, and are wired with compensation adjustments as shown in Figure 7-2. When
weight is applied, the strain changes the electrical resistance of the gauges in proportion to the load. Other load cells are fading into
obscurity, as strain gage load cells continue to increase their accuracy and lower their unit costs.
Choose the right load cell for your application
S-Beam Load Cells
A S-Beam load cell get its name from its S
shape. S-Beam load cells can provide an output if under tension or compression. Applications include tank level,
hoppers and truck scales. They provide superior side load rejection.
Canister Load Cells
Canister load cells are used
for single and multi-weighing applications. Many feature an all stainless steel design and are hermetically
sealed for washdown and wet areas.
Frequently Asked Questions
Load Cell Performance Comparison
Type |
Weight Range |
Accuracy (FS) |
Apps |
Strength |
Weakness |
Mechanical Load Cells |
Hydraulic Load Cells |
Up to 10,000,000 lb |
0.25% |
Tanks, bins and hoppers.
Hazardous areas. |
Takes high impacts,
insensitive to temperature. |
Expensive, complex. |
Pneumatic Load Cells |
Wide |
High |
Food industry, hazardous areas |
Intrinsically safe.
Contains no fluids. |
Slow response.
Requires clean, dry air |
Strain Gage Load Cells |
Bending Beam Load Cells |
10-5k lbs. |
0.03% |
Tanks, platform scales, |
Low cost, simple construction |
Strain gages are exposed,
require protection |
Shear Beam Load Cells |
10-5k lbs. |
0.03% |
Tanks, platform scales,
off- center loads |
High side load rejection, better
sealing and protection |
|
Canister Load Cells |
to 500k lbs. |
0.05% |
Truck, tank, track, and hopper scales |
Handles load movements |
No horizontal load protection |
Ring and Pancake Load Cells |
5- 500k lbs. |
|
Tanks, bins, scales |
All stainless steel |
No load movement allowed |
Button and washer Load Cells |
0-50k lbs
0-200 lbs. typ. |
1% |
Small scales |
Small, inexpensive |
Loads must be centered, no
load movement permitted |
Other Load Cells |
Helical |
0-40k lbs. |
0.2% |
Platform, forklift, wheel load,
automotive seat weight |
Handles off-axis loads,
overloads, shocks |
|
Fiber optic |
|
0.1% |
Electrical transmission
cables, stud or bolt mounts |
Immune to RFI/EMI and
high temps, intrinsically safe |
|
Piezo- resistive |
|
0.03% |
|
Extremely sensitive, high
signal output level |
High cost, nonlinear output |
↓ View this page in another language or region ↓