AR-EP, AR-LT Series
These models add a weatherresistant
enclosure (AR-LT series)
or an explosion-proof enclosure
(AREP series) to the AR Series
shown in the P Section. With the
exception of the enclosure type,
specifications are the same as listed. AR-EP models are UL listed
for use on Class I, Groups C and D,
and Class II, Groups E, F and G
hazardous locations.
Caution–Hazard of Fire:
Types AR, ARR, AR-LT and AR-EP
thermostats do not provide failsafe
temperature controls for heating. If
the thermostat bulb ruptures, the
controller senses that the temperature
is not at the setpoint and heat stays
on. A backup high limit temperature
controller is recommended for safety.
*Not intended for use in hazardous areas.
† All prices on this site are shown in Thai Baht.
We noticed you are from the US. Visit your local site for regional offers and live support.