The OS-XL has been discontinued, please see the OSXl-TIC Series or the OSXL-EX as possible substitutes or consult OMEGA's Temperature Engineering department.
This product has an Interactive Showcase. Click on the icon to the left to experience it.
The OS-XL displays an image of the measured
subject and the temperature distribution at 64 measurement points.
The most advanced temperature gage—brought to you by
The OS-XL is a 2-dimensional infrared
thermometer equipped with a newly
developed 64-element thermopile array
sensor. The OS-XL is not just another
non-contact temperature measurement
device–the OS-XL allows the user to
view and verify the measurement
subject on the LCD screen while
simultaneously measuring the
temperature at 64 points. The OS-XL
can actually display and save data with
a graphic representation of the
temperature distribution overlaid on an
image of the subject being measured.
Furthermore, device operation is
extremely easy, similar to that of a
digital camera, greatly increasing
operation efficiency. The OS-XL offers
exceptional functionality that has never
been available before at this amazingly
low price. Combining OMEGA’s
original technologies and concepts,
the OS-XL takes the lead in the field
of temperature measurement.
The Newly Developed 64-Element Thermopile Array
A thermopile is the heart of most of today's leading infrared
thermometers. The Thermopile Array consists of a matrix of multiple
thermopile elements, but attempts to put this technology into practical
application have been hindered by size and sensitivity problems. OMEGA
has managed to overcome these problems using semiconductor
processing based micromachining, successfully developing a micro-size,
high-sensitivity thermopile. The resulting 64-element Thermopile Array
consists of an 8 x 8 matrix of 0.5 mm2 (0.02"2) elements, the first such
matrix in the world to be put into practical application.
The true value of the OS-XL lies in its ability to
display temperature distribution on an image
of the measurement subject.
The image of the object being measured is divided
into a 64-frame grid. The temperature distribution is
displayed in corresponding colors on the grid lines
framing each area. Temperature is measured in each
frame. The cursor can be used to select a specific
frame in order to display the temperature for that area in
0.1° increments. The OS-XL provides easy operations
for both measuring and recording data. The OS-XL also
provides a diverse range of settings functions and data
options supporting "smart temperature measurement"
with its enhanced functionality.
All recorded data is saved on a Compact Flash (CF) card.
All recorded data is saved on a Compact Flash (CF) card.
The OS-XL is equipped with a Compact Flash card slot so that image
data and measurement data can be easily saved and stored. All of the
measured values for each grid frame are saved for each image. The
OS-XL can simultaneously record data for 64 measurement locations.
(Images are saved in JPEG format, and measured values are
saved simultaneously as a CSV-format file.)
The OS-XL saves data in formats
that can be easily edited by computer.
The data saved on the CF card can be read by most
computers. It is easily viewed and edited without
using specialized software. With Microsoft Excel, the
image and measurement data can also be analyzed
and used to generate illustrated reports.
Measurement conditions can be easily recorded using the OS-XL's video output
The OS-XL is equipped with a video output jack, so the measurement conditions
can be easily recorded on videotape or monitored on a large-screen TV.
(Please use the video cable included with your unit for video output.)
Easy Operation, with the Feel
of a Digital Camera
In addition to making measurements, the OS-XL also makes
it easy to save data—just line up the object being measured
in the LCD monitor and press the "Save" button. The
lightweight, compact body of the OS-XL makes it an
exceptionally convenient measurement device.
A Diverse Range of Applications in a Wide Variety of Fields
Caution: This product and all in the series are not for use in medical evaluations. These products cannot be used to measure body temperature. They are meant for industrial and scientific purposes.
† All prices on this site are shown in Thai Baht. Note: Unit comes complete with 16MB Flash Card, Flash Card reader, hand strap, 6 AA alkaline batteries, AC adaptor, carrying case, video cable and complete owner’s manual.
We noticed you are from the US. Visit your local site for regional offers and live support.