Originally, the idea was to replace RS232 cables with Bluetooth wireless. Later, Ericsson, Nokia, Intel, IBM and Toshiba formed the Bluetooth Special Interest Group to further the use of the technology.
Bluetooth uses radio waves to transmit data over short distances, up to 328 feet or 100 meters, although most devices have a more limited range closer to 30 feet due to interference. Bluetooth technology transmits in the 2.4 to 2.485 GHz range. It is a spread spectrum, frequency hopping full-duplex signal.
Bluetooth wireless requires a chip to transmit the radio signal and software to enable connections. It has a uniform standard for connection that has contributed to the proliferation of Bluetooth, and as a result, it is in a vast array of devices, from mobile phones to cars to medical devices and fitness monitors. Bluetooth is widely expected to play a key role in the evolving Internet of Things (IoT)
Pros of Bluetooth Wireless
- Low power so it works well in battery driven devices
- Inexpensive so it can be deployed in low cost devices
- Manages voice and data transmissions simultaneously
- Low latency
Cons of Bluetooth Wireless
- Limited range in most devices
- Data transfer rate (24 Mbits/s)
- Incompatible pairing protocols between devices
- Requires local data logging to ensure uninterrupted data availability
Bluetooth Models
UWBT Series available in Thermocouple, RTD, Relative Humidity & Temperature, and pH & Temperature models. RTD and thermocouple transmitters available with M12, or uni-connectors.