CTPH
pH & Temperature Chart Recorder, Microprocessor-Based
† All prices on this site are shown in Taiwan Dollars.
Note: Comes in a charcoal gray color, with detachable solid state pH/temperature sensor, additional 6 ft. extension cable, 120 double-sided charts (40 each of 1,7,32 Day), two sets of pens, wall mount template and hardware, 110 or 220 Vac adaptor, chart lights, 4 “D” alkaline batteries and complete operator’s manual.
Using the BNC adapter, CTPH-BNC, the ATC is disabled and any low cost pH sensor can be employed, like laboratory type PHE-4202.