The EZ220 and EZ420 series has been discontinued. Please see the GP Series as a possible alternative or contact our Automation Engineering department.
EZ Series Textpanels are Easy to Operate
EZ Series Text Panels and
EZ Series Text PLCs have been enhanced to
incorporate a vacuum fluorescent
display that has greater visibility as well
as a wider viewing angle.
Multi-Color Annunciator LED Lamps
The annunciator lamps on the EZ-220P
and EZ-220PV models are configured
similar to pushbuttons. Once you have
selected the starting address in the
PLC, all of the lamp colors will be
identified by the bit pairs. The color that
the lamp illuminates depends on the bit
assignment of the address selected.
256 User Programmable Messages
There are two message types which
can be displayed: local and PLC. Local
messages are displayed on the screen
unless the PLC triggers a PLC
message, which overrides a local
message.
PLC Message LED Indicator
When a PLC message is triggered, the
PLC Message LED will also be
illuminated. The PLC message LED will
remain on until the user acknowledges
the situation by pressing [esc] on the
panel.
NOTE: Programming software (EZ-SERIESEDIT-E) and programming cable (EZ-SERIES-PGMCBL) required.
† All prices on this site are shown in Taiwan Dollars.