Thermocouple wire is used to measure the temperature electronically. Two wires of different metal joined together at the sensing end to measure the temperature. Low voltage signal is measured in thermocouple by using wire from the point of sensing to the point of cold junction compensation (cjc end). Different combination of metal wires are used in different thermocouple types such as J, K, T, E, etc.
The four most common types are J, K, T and E. There are high temperature thermocouples R and S. Each type has a different sensitivity (gain), linearity, temperature range and environment, although the maximum temperature varies with the diameter of the wire used in the thermocouple. Thermocouple type defines the temperature range, the maximum range is also limited by the diameter of the thermocouple wire.
Bare Thermocouple Wire
Duplex Insulated Thermocouple Wire
Metal Sheathed Thermocouple Wire
↓ View this page in another language or region ↓
Fios para Termopar
Fils de Thermocouple
Alambre de Termopar
Alambre de Termopar
Thermocouple Wire
Termokoblerkabel
Fils et Câbles de Thermocouple
Thermoelementleitung
Cavi per Termocoppie
Thermocouple Wire
Cable termopar
Thermocouple Wire
Thermocouple Wire
热电偶线
Thermocouple Wire
熱電対線
써모커플 와이어
Thermocouple Wire
Thermocouple Wire
Thermocouple Wire
Thermocouple Wire
Thermocouple Wire