More»
 Accessibility  Skip navigation  Site Map  Help  Search field  View shopping cart  View shopping cart  Skip to Navigation

Current Multiplexer

DRA-CSM-1   
1 year warranty OmegaCare
 
Current Multiplexer
DRA-CSM-1:Current Multiplexer
Click for larger image.
   
$1,435.00  DRA-CSM-1
Multiplexes Sixteen 4-20 mA Inputs Into One 4-20 mA Output
± 0.01% Accuracy
Channel Selection Controlled by 4 Discrete Inputs
Solid-State Technology
Economical PLC Upgrade

View related products - Signal Conditioners

Click to scroll below to order See Specs PDF Manuals

The DRA-CSM-1 Current Multiplexer is a solid state multiplexer capable of transferring the selected 4-20 mA input current signal to the output terminals in less than 10 microseconds at an accuracy better than 0.01%. The DRA-CSM-1 is typically controlled by a PLC thereby obtaining full data synchronization. The DRA-CSM-1 is provided with a unit enable/disable control line which enables the parallel connection of several multiplexers to the same controller input. The period during which the unit is disabled is used for self-testing according to a self-test procedure which checks the unit’s hardware. Model DRA-CSM-1 is powered by an external DC power supply. Each two-wire 4-20 mA transmitter is connected to the input terminals. Each channel provides a current limited voltage supply for the connected two-wire transmitter. The channel selected by the multiplexer is directed to the control device’s (e.g., PLC’s) analog inputs. Power is maintained by the multiplexer to the unselected channels thereby maintaining uninterrupted transmitter current flow. Each 4-20 mA input channel on the multiplexer has its own red LED status light which illuminates on presence of current in the loop.


To Order (Specify Model Number)    
expand list What Other People Bought: When you see this icon, click on it to expand a list of products that other people have bought when they purchased this model.
 Part Number   Availability   Price   Description    Qty.
    DRA-CSM-1 2 weeks   1,435.00    Current multiplexer  
Click to expand/minimize a list of what others bought with the iDRN-PS-1000  iDRN-PS-1000    Consult sales   Power supply, 95-240 Vac input, 24 Vdc @1A output  
All dollar amounts on this site are shown in Singapore currency.

 Note: Comes with complete operator’s manual.

   
Keywords:Current Multiplexer, movement sensors

   Back to topBack to top