Image coming soon
Variable Area Flow Meters
... case or end fittings the application can demand, so as best to meet customer requirements. ... The practical temperature limit for glass variable area flow meters is 204°C (400°F), ...
https://sea.omega.com/th/prodinfo/variable-area-flowmeters.html - 73K - 6/19/2026
Image coming soon
Infrared Thermometer
... The best known and most commonly applied of these designs is the Two Color-Ratio ... It originates in the old practice of relating visible color to temperature, hence "color ...
https://sea.omega.com/th/prodinfo/infraredthermometer.html - 89K - 6/19/2026

Customization Process of Pressure Transducers and Load Cells
... Best practices for simple customization Once you determine that making simple modifications to a standardized product is the best investment for your application, it's time to ...
https://sea.omega.com/th/technical-learning/right-expertise-can-simplify-customization-process.html - 73K - 6/19/2026

Ultrasonic Level Sensors in Above Ground Bulk Storage Tanks
The distance is then converted into a percentage of measured span and output as a proportional 4-20 mA signal. Best Practices The installed level sensor must have a clear view of ...
https://sea.omega.com/th/technical-learning/ultrasonic-level-transmitters-in-above-ground-bulk-storage.html - 73K - 6/19/2026

Considerations Before Installing Sensors in Piping Systems
Because sensor accuracy will be compromised by an immersion depth that is less than ideal, it is best practice to have an immersion probe depth of at least 15 times the diameter of ...
https://sea.omega.com/th/technical-learning/invasive-sensor-considerations.html - 65K - 6/19/2026

What is MI Cable?
Note: Consult with MI cable manufacturer for their recommended insulation best practices. MI Cable with Thermocouples and RTDs MI cable is typically used in the construction of ...
https://sea.omega.com/th/technical-learning/what-is-mi-cable.html - 70K - 6/19/2026

Cryogenics
... Selecting a sensor to a specific temperature range is the best. Calibration of the sensor and the instrument is a good practice. Sensor Location If the sensor and the application ...
https://sea.omega.com/th/prodinfo/Cryogenics.html - 74K - 6/19/2026

Pressure Transducers and Transmitters
voltage and 4-20mA. Below is a summary of the outputs and when they are best used. ... making your decision, this article, Practical Considerations when Choosing a Pressure ...
https://sea.omega.com/th/prodinfo/pressuretransducers.html - 78K - 6/19/2026

Automating food processes ensures quality & safety standards
... "Having the level of controls and the automation to produce the product as best in class ... Best practices in practice. For the FIC, it's critical that their clients work in a ...
https://sea.omega.com/th/technical-learning/automating-for-food-quality-and-safety-standards.html - 70K - 6/19/2026

Variable Area Flow Meters
... case or end fittings the application can demand, so as best to meet customer requirements. ... The practical temperature limit for glass variable area flow meters is 204°C (400°F), ...
https://sea.omega.com/th/prodinfo/variable-area-flowmeters.html - 73K - 6/19/2026

Infrared Thermometer
... The best known and most commonly applied of these designs is the Two Color-Ratio ... It originates in the old practice of relating visible color to temperature, hence "color ...
https://sea.omega.com/th/prodinfo/infraredthermometer.html - 89K - 6/19/2026