Cart  |  Contact  |  Help  |  seainfo@dwyeromega.com  | 
Toll-Free in Thailand: 001 800 441 0237
International+65 6415 5353

Optimizing Strain Gage Performance for Inhomogeneous Materials

Using Strain Gages Strain is the deformation of a material resulting from applied force, and it is measured by change in length. It can be either tensile or compressive. A strain gage is a device that varies its electrical resistance in proportion to strain. Strain may result from a number of internal or external influences, including pressure, temperature, or structural change. The most commonly used gages are bonded metallic strain gages, which consist of fine wire or foil assembled in a grid pattern. The grid is bonded to the test specimen and detects changes in length that occur when a load is applied. This leads to a change in resistance, which is measured by an electric circuit. Inhomogeneous materials may present numerous complexities in obtaining accurate strain measurements.

Properties of Inhomogeneous Materials

Until recently, the majority of strain measurements were applied to metals such as steel and aluminum alloys. The current trend of replacing metals with polymers and composites has brought about a growing number of reinforced plastics with significantly different mechanical, thermal, and chemical properties. One major difference in the physical properties of metals and polymers is found in the elastic modulus. A composite material with a polymer or plastic matrix may have an elastic modulus of more than twice that of metals, depending on the fiber material and volume of reinforcement. As a result, strain measurements for these inhomogeneous materials are considerably larger than for metals and usually require special strain gage bonding and wiring techniques.

The thermal conductivity of polymer matrix composites can be as much as two orders of magnitude lower than that of metals. When the test specimen and gage undergo deformation, the gage resistance changes in response to strain and generates a calibrated voltage offset. Strain gages with a higher resistance result in less heating for the voltage produced. However, polymer matrix composites do not conduct heat well and may allow heat to accumulate in the gage. This increase in temperature causes an increase in resistance and, subsequently, an error in strain measurement. In some cases, this may require temperature compensation.

Some inhomogeneous materials are hygroscopic and may expand or contract as moisture content changes. These dimensional fluctuations are not differentiated from thermal output and result in false strain measurements. Plastic composite matrices vary significantly in hygroscopic properties. For example, acrylic plastic has a strong tendency to absorb moisture, while polyethylene absorbs practically no moisture. Wood is another inhomogeneous material prone to absorbing moisture. Wood will expand and contract with atmospheric changes. Additionally, the shrinkage that occurs during drying is less in a direction parallel to the grain than in a direction across the grain. This underscores the necessity of proper specimen selection for compensating strain gages as well as providing consistent atmospheric conditions for both the active and compensating gages.

Gage Length for Inhomogeneous Materials

The gage length is defined as the receptive region of the grid. Solder tabs and end loops are excluded from what is regarded as the strain sensing area of the gage due to the comparatively large size of their cross-sectional area and low electrical resistance. Strain gage lengths are typically selected based on the size and shape of the sample and anticipated strain distribution. The gage length also plays an essential role in the accuracy of strain measurements. Strain gages of 0.125 inches or greater usually provide greater stability and measurement range. Additionally, larger gages provide better heat dissipation, since they have a lower wattage per unit of grid area.

Gage length is also an important consideration in strain measurements for inhomogeneous materials such as reinforced plastics and concrete. The length should be large in relation to the size of the inhomogeneities in the sample to provide strain measurements representative of the structure. Measurements of inhomogeneous materials usually seek an average strain rather than the inconsistencies that arise at the peripheries of aggregate and matrix materials.

Gage Pattern

Choosing the right gage pattern is crucial in optimizing strain measurements. The gage pattern designates the configuration of the grid and solder tabs. Grid width may be either narrow or wide, depending upon the application. A narrow grid width minimizes the averaging error for strain gradients aligned vertically to the gage, while wider grids facilitate heat dissipation for specimens that exhibit poor heat transfer properties. The solder tab configuration should concur with the size and position of the installation and allow the connection of lead wires.

Frequently, identical gage patterns are offered with a different resistance; the most common are 120 and 350Ω. The higher resistance gage is most often preferred because it decreases the amount of heat generated and reduces signal noise from lead wires and other sources of resistance changes.

Adhesives

TT300, SG401, SG496 Strain Gage Adhesives
TT300, SG401, SG496 Strain Gage Adhesives
Adhesive selection can affect the performance of the strain gage, since it essentially becomes part of the measurement system. Therefore, it is advisable to use adhesives recommended by the gage manufacturer. Epoxy adhesives that cure at room temperature are acceptable for most inhomogeneous materials, such as composites. They are available in multiple formulations, with properties to accommodate variations in temperature, time, and elongation capability. If you are applying an epoxy to glue composite sheets together, the epoxy used would be a good choice to adhere the gage. Unfilled adhesives are normally preferred to minimize creep. However, composite materials with fibers that result in an irregular surface may present difficulties in bonding. In such cases, a partially filled adhesive may be applied to smooth the surface prior to bonding the specimen to the gage with unfilled adhesive.

Strain Gages Designed for Inhomogeneous Materials

SGD-30/120-LY40 Extra-Long Strain Gage
SGD-30/120-LY40 Extra-Long Strain Gage
The OMEGA® SGD-30/120-LY40 is an extra-long strain gage designed specifically for inhomogeneous materials. Its grid measures 25 by 8 mm, and the carrier is 40 by 12 mm. The nominal resistance is 120Ω, and it terminates with solder pads. Constantan foil is used to form the grid, which is sealed in a polyimide carrier. OMEGA’s SGD-30/120-LY40 is flexible and strong to provide highly accurate static and dynamic measurements.

The SGD-30/350-LY40 strain gage is made from the same quality materials as the SGD-30/120-LY40. Its 50 mm length improves the accuracy of strain measurements for inhomogeneous materials. The grid is 30 by 3 mm, and the carrier is 36 by 5 mm. Nominal resistance for the SGD-30/350-LY40 is 350Ω. This linear pattern strain gage is designed to measure strain in a single direction.

Conclusion

SG1-KIT Strain Gage Application Kit
SG1-KIT Strain Gage Application Kit
Extra-long strain gages provide several advantages for strain measurements of inhomogeneous materials. They support a larger area for measurement, which allows a better representation of the material’s structure. In addition, the greater surface area facilitates heat dissipation to deliver more stable measurements.

WHITE PAPER
Download the complete white paper about
Using Strain Gages
Related topics
Strain Gage
Strain Gage for Inhomogeneous Materials | Related Products